2024-10-25 7:22 AM
2024-10-25 9:31 AM - edited 2024-10-25 9:32 AM
Earlier post, you don't need to post things three times.
https://community.st.com/t5/other-hardware/diode-g86-need-data/td-p/735765
Marking hard to read, is the second diode on the board the same?
Are we sure these are authentic? marking look awfully rough
ST DIODE 68B
ST DIODE G8B
Wrong style for BZW50-68B axial
Perhaps SM15T68A ?
2024-10-25 12:40 PM
It’s really hard to read, but it is GB6 = STPS1L60A, a Schottky in SMA.
Hope that helps?
Regards
/Peter
2024-11-05 12:46 AM
Good morning.
I apologize for the delay, have tried and it is not working.
it should start clipping at approximately 82 volts according to a unit that is still working
Thank you
Denis Norton
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.