Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hello, we are searching for a USB PD Power Budgeting/ Load Sharing solution. Here an example: Lets say we have 4 USBC PD Ports. All in all they sould be able to source 60W. One port is sourcing 15V/3A=45W, then the remaining 4 should just be able to ...
I am designing an interface board where there is an ADC that needs two different power supplies (3.3V and 2.5V). To minimize this board, instead of bringing the two power supplies from outside, I would like to bring only the 3.3V one and through a vo...
Hi, I am currently implementing software/firmware for the PowerSTEP01 chip and discovered a inconsistency in data sheet https://www.st.com/resource/en/datasheet/powerstep01.pdf. For parameter INT_SPEED (section 11.1.11 in datasheet) the equation does...
According to the reference circuit, R43 is 75kohm.Also UM2154 User manual said that R43 should be higher than 30kohm.What happens if R43 is 22kohm. Is overcurrent detected by STSPIN32F0?
HelloI need to estimate IFSM for certain current pulse.Does anyone know how to do it?I found this app note :Schottky diode avalanche performance in automotive applications (st.com)But it is not clear the method as intervals are weird :I ^4 x t = Cste...
Regarding the shunt resistors connected to the SENSEA and SENSEB pins, the UM1829 has three 0.1 ohm resistors connected. Why is this? The datasheet says one 0.1 ohm resistor.Do I really need three of them?
Hi, Can PD Controller (STUSB4710) act as a DRD?STUSB4710 - Stand-alone USB PD controller (with short-to-VBUS protection) - STMicroelectronicsI believe that STUSB4710 cannnot operate as DRD (Dual Role Data), and can only function as UFP.If there is a ...
Hey, probably a dumb question, but I couldn’t find it in the datasheet. Can each pin of the VNQ9025AJ handle 30A, or is that the rating for the smart switch as a whole with a limit on each pin? Honestly, I’m hesitant to believe a single pin can handl...
I know this is a really dumb question, but I cannot find a definitive answer in the datasheet for the VNQ9025AJ, Quad channel high-side driver with Current Sense analog feedback for automotive applications.There are 4 pins called INPUT0 to INPUT3. Th...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.