2014-12-02 4:41 AM
Hi. I'm trying to find application notes that relate directly to the EVAL6229PD. All I have been able to find is application notes for the EVAL6235N and they do not relate directly to the 6229 as it has a different layout. Any help would be appreciated.
#eval6229pd #application-notes2014-12-03 7:34 AM
The L6229 is the same of the L6235 but the current rating, so you can use the application note AN1625 as reference for the device operation.
In the AN the only board listed is the EVAL6235N, but also in this case the board is very similar to the EVAL6229PD.2014-12-04 8:31 AM
Hi Enrico. Thanks for that. So does the EVAL6235N have a higher current rating than the EVAL6229PD? The application note seems to indicate that the maximum current is 2.8A RMS and 5.6A peak but when we run the software we are limited to about 1.5A.
Thanks2014-12-15 5:52 AM
Correct. The L6229 is the ''low power'' version of the L6235 but they share the same control circuitry.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.