2021-05-02 2:37 AM
I'm currently prototyping with the Steval-ISV019V1 (evaluation board for SPV1050) and have only changed the resistor ladder for MPPT. Energy harvesting works nice.
But when I enable one of the LDOs and have > 4-6uF connected on the LDO output, the LDO voltage collapses to around 0,8V. When I remove the capacitive load it takes a few seconds until it is possible to enable the LDO again and it starts working normal (stable 3.3V output).
Is this a normal behaviour of the SPV1050? I suppose not, may the chip is destroyed?
May someone can help with its knowledge?
Thanks!
2021-05-03 3:12 AM
Update: I'm not able to measure it, but the problem seems to be the current spike at t0 when connecting the capacitor (even it is a very small one).
When I add a 33Ohm resistor (theoretical I max = 100mA) in serial to the capacitive load the LDOs voltage is and stays stable.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.