2019-01-15 6:16 PM
I have a project where I would like to drive two separate sensored BLDC motors with a single microcontroler. The only options I have seen involve the control of a single motor with no options of stacking shields (in the Nucleo's case) or using multiple motor control connectors (ie STEVAL-IHM028V2)
There is also an additional option using the STEVAL-IHM034V2 board in conjunction with an additional STEVAL-IHM034V2 power board. I have to dismiss this option since I an working on a low power proof of concept and would like to have encoder feedback.
I was wondering if there where any additional hardware configurations that I may have missed?
2019-01-24 9:42 AM
Dear Javilen,
one tip: If you want to get the dual board configuration we use and tested in ST using ST MC Workbench. Go to "New Project" and select Dual Motor (step 2) .
Best regards,
Claire
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.