2018-08-15 6:01 AM
I'm currently working in a project where I need to control the intensity of 24 high power LEDs in 5 levels. I'm planning to use LumiLeds L1CU-BLU1000000000 (https://www.lumileds.com/uploads/705/PB198-pdf) where the cut-off voltage is 2.83 volts and current is 350mA. As per the requirements, the power supply should be from an SMPS ( maximum output - 12v,6A).
I need to select a constant current driver with PWM facility ( 0-5v max ) to control the LED intensity from a micro-controller. What type of driver IC will be best suit for this application?
What I know so far is:
If I'm using 3 driver ICs and dividing up the LED load among those, is it still okay to use 3 pwm channels from the micro-controller for dimming all the LEDs simultaneously? I'm planning to use STM32f4 series micro-controller in my project, I hope that it can drive 3 PWM channels at a time.
I've searched and found one IC, but still I doubt whether it will suit my application or not.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.