2026-03-07 12:23 AM - last edited on 2026-03-07 2:11 AM by Andrew Neil
Hello,
We are currently integrating the SPSB081 PMIC for voltage and wake-up management in a Body Control Module (BCM). The PMIC is interfaced with an NXP S32K312 MCU via SPI.
System Setup:
Issue: Watchdog Runtime Configuration
We are trying to perform runtime watchdog configuration and set the watchdog window to 160ms. However, we would like to confirm the correct SPI command sequence required for modifying the watchdog configuration during runtime.
Request:
Thank you
2026-03-07 6:33 AM - edited 2026-03-07 6:34 AM
The datasheets says to set WD_CONFIG_EN and then set WD_TIME. That's what I would do.
There are two watchdog timings available. Neither are 160 ms.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.