2021-02-15 2:38 AM
Hello everyone,
I have a problem, to ensure GPIO initialisation after a wake-up from standby mode...
if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
{
HAL_PWREx_DisablePullUpPullDownConfig();
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); // clear du flag standby
HAL_PWR_DeInit(); // Réinitialise la configuration Power à zero
__HAL_RCC_PWR_CLK_DISABLE();
}
//init My GPIO but it dosen't works..I have the same problem for my 3 GPIO pins, if someone have a idea ?
Thanks for reading.
2021-02-15 5:07 AM
Hello @Quentin_27 and welcome to the ST Community.
For a better support, could you share more information about the hardware you are using?
2021-03-04 12:47 AM
Hello @Quentin_27,
any update about your issue?
Are you using a standalone MCU or a System-In-Package with embedded microcontroller?
For a better support could you share the part number of your device?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.