2022-06-26 6:07 AM
We are using NFC tag with 0600-00061 antenna from Laird connectivity and charging coil WR121210-27M8-ID from TDK with wireless charging IC STWLC38JR .
Will it be okay to use both and will they work alright?
2022-06-27 2:03 AM
Hi plawat,
which tag are you using on the 0600-0061 antenna?
BR, Ulysses
2022-06-27 2:06 AM
We are using Nordic nrf5340BLE SoC in our design. This also has a function to be used as NFC tag. We are using this functionality of nrf5340.
2022-06-27 2:07 AM
We also are searching for some help in miniaturizing the antenna design to be used with nrf5340 as our requirement of tag sensing distance is 1cm only.
2022-06-27 5:02 AM
Hi plawat,
there are two considerations:
Best Regards, Ulysses
2023-09-21 12:44 AM
Hi, In our smart ring design we are integrating the ST25DV based charging solution for our 28mAh battery. We need to have a printable NFC charging tag to be incorporated in our design so that the size adn footprint is reduced. WE need the gerber / schematics for the same.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.