2021-06-22 9:14 PM
Hello, I am trying to use L6470 for stepper motor control.
I tried to change L6470's step mode register from 0x07(reset value) to 0x05.
But when I read it back after I sent a command, its value was the same.
I use 6 L6470 chips but this problem happened to only 2 chips.
This means the firmware was correct but there are some problems with my PCB board.
Thus, Here I have a question about the register setting.
Which situation cause this problem?! is there anybody who knows about this?
Solved! Go to Solution.
2021-06-23 11:37 PM
Hi @Jhan.1 and welcome to the ST Community.
Could you share more details on your application?
Are you using a custom board and/or custom firmware?
For now I can suggest to refer to the application notes AN4290.
In the paragraph 2 you can find more details on the daisy chain connection and configuration to drive multiple devices with a single SPI interface.
EDIT: please not that the STEP_MODE register is writable only when outputs are in high impedance.
Let me know if these info are useful to you.
2021-06-23 11:37 PM
Hi @Jhan.1 and welcome to the ST Community.
Could you share more details on your application?
Are you using a custom board and/or custom firmware?
For now I can suggest to refer to the application notes AN4290.
In the paragraph 2 you can find more details on the daisy chain connection and configuration to drive multiple devices with a single SPI interface.
EDIT: please not that the STEP_MODE register is writable only when outputs are in high impedance.
Let me know if these info are useful to you.
2021-06-28 4:49 PM
Thank you Cristiana, your answer really helped me!!
As you suggested, when I let L6470 be Hi-Z state, I can write registers.
Maybe there were some problems when it turned on.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.