2014-01-26 8:12 AM
I want to use the L6206 to drive 4 solenoids (one end of the solenoid each solenoid will be grounded) of 2.5amps each. Can this be done without damaging the IC. ? Also each of the bridges two halfs will not be drived simultaneously. Means the 2 solenoids on 1st bridge will be used only alternatively and never simultaneously. Can this be done?
In a case if both bridges are simultaneously turned on the data sheets says it will have Vs on its output pins, I had a question if this condition though it would not ever occur would be bad for the circuit reliability.Thanks2014-03-11 1:32 AM
Ciao
I suggest to post this question in the forum. Thanks Ciao GigiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.