2015-04-09 12:02 PM
The new version (V2.2 stsw-spin002.zip) has a much improved setting of motor paramaters, and it now works on XP but the GUI still crashes badly so motors cannot be tested.
# GUI crashes hard in both XP and Win 7, in XP = unhandled exception and program terminates # loses comms between board and PC and must close GUI and restart # loses communicatinos when motor is run for an hour # SPEEDregister reads correct value (0.998 s/s), but GUI reports 67 steps per second and reports 670 s/s when motor is running at 10 s/s # GUI will not accept changes in microstep rate # Command error reported in GUI when attempting to pass paramaters to the board. # in setup window (to set motor paramaters), GUI repeatedly crashes in testing ADC level # loss of comms between PC and board when motor runs a long time # false register values indicated in Register Map window GUI has been removed and reinstalled on both XP and W7 machines, still doesnt work.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.