Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VN5050AJ CS_DIS not working - again

As in https://community.st.com/t5/power-management/vn5050aj-cs-dis-not-working/m-p/632201#M10745 we now have added seriel diodes for every chip, but it is still not disabling his Current_Sense Output altough the CS_DIS Pin is above 3V.  The CS_DIS-1 ...

vn5050DisableCS.png
rkager by Associate II
  • 1243 Views
  • 1 replies
  • 0 kudos

STSPIN230

Hi, We are using STPIN230 Motor driver in our applicationOur BLDC Motor electrical parameters are:1) Rotor inductance - 0.11 mH2) Terminal resistance - 10.7 ΩQueries we have:1) In our current design we have STSPIN230 connected to motor as follows( in...

NIVI_0-1721224287584.png
NIVI by Associate III
  • 826 Views
  • 0 replies
  • 0 kudos

STC3117 get Gas gauge charge data

  Hi,I'm using the STC3100 chip to get the coulomb used from the battery, using the REG_CHARGE_LOW registers,on the new board, I want to move to STC3117, but I don't see this register,Does anyone know how I can get this value? ThanksShamir

Fuel Gauge for 2s1p 7.2V

Dear Experts  I am using 2s1p  PA-LNB76-C17UL.4.1.R001 battery, Panasonic NCR18650BF battery for my new application.  Output Voltage - 7.2VCurrent - 3350mAhI would like to know a compatible fuel gauge IC for it. Please pour your suggestions. Kind Reg...

DA24 by Associate
  • 1919 Views
  • 2 replies
  • 0 kudos

Resolved! Error Flashing firmware to STWLC98

Hello,I have developed my own evaluation Board for the STWLC98 Chip. When connecting the power suplly, the DC-Mode, which is on the IC when it is delivered, works in a correct way. But when I want to program the IC with the following firmware from th...

simonh by Associate III
  • 3885 Views
  • 5 replies
  • 0 kudos

Resolved! EVALSTDRIVE101 - Questions about FET's gate circuits

Hello,I use ST's STDRIVE101 in a design to drive a three-phase BLDC motor and used the reference design EVALSTDRIVE101 as a design guideline. My design has a MOSFET switching frequency of 20 kHz and a MOSFET drain-source voltage between 36 and 42 V.I...

mual_0-1720432029231.png
mual by Associate
  • 1883 Views
  • 2 replies
  • 0 kudos

L6470 Low Speed

Is it possible to program the L6470 MIN_SPEED for a low value, set the acceleration and deceleration to zero and MAX_SPEED to zero to run at the set MIN_SPEED rate?

tborgoyn by Associate
  • 712 Views
  • 0 replies
  • 0 kudos

LED2001PHR based driver does not work

Posted on December 30, 2017 at 11:16I have a LED2001PHR based LED driver that is designed to drive a string of LEDs at 5.2V and 3A. When I apply power and the LEDs are connected, the LEDs flash for a fraction of a second and then go off telling me t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.