Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Thermal resistance information ST6710

Hello,I need some information on the thermal resistance Rthja and Rthjc of the STM6710 (package SOT23-6L). Could you please send some technical information like a datasheet which we can forward to certification authority?I often miss this information...

WEmme by Associate II
  • 1218 Views
  • 2 replies
  • 0 kudos

L6482 current control parameters

Hi,I am concerning about the L6482 current control parameters that are explained in the AN4158.I assume that tSW, tON_MIN, tOFF_MIN, tOFF_FAST, tFAST_STEP reflect the relevant registers. So:1. Peak current control with auto adjusted decay: - tOFF: th...

huytung1501_0-1719988900013.png huytung1501_1-1719989153958.png huytung1501_2-1719989209540.png

Resolved! WBC2TX50 board does not go past FSM_PRE_PING_STATE

I have a WBC2TX50 eval board along with a STEVAL-WLC98RX for testing Qi powe transfer. When I try to make the transfer, the WBC2TX50 board does not go past FSM_PRE_PING_STATE, either with the WLC98RX or with a phone, both of which work with a standar...

AMG by Associate
  • 1553 Views
  • 1 replies
  • 0 kudos

Vipergan50TR, switching frequency

Dear ST office, I have a project with the chip Vipergan50TR.We need the output voltage of 20V/0.2A,  -20V/0.2A,  7V/1.5A. We plan to let the vipergan chip control 20V channel. I tried your online design tool for AC/DC. When i typed in output voltage ...

Resolved! DIODE IDENTIFICATION

HI.I'm looking for this diode so I can change it.I need the order number to buy it.  

MP_7_0-1721494141359.png
MP_7 by Associate
  • 1237 Views
  • 1 replies
  • 1 kudos

STEVAL-WLC38RX transmit data to STEVAL-WBC2TX50

Hi, it seems that the STEVAL-WLC38RX uses STSW-WPSTUDIO and the STEVAL-WBC2TX50 uses STEVAL-WBC2TX50. Is it possible to program the STEVAL-WLC38RX to take external ADC measurements via the NTC pin or the GPIOs and send it to the STEVAL-WBC2TX50 using...

JMin.17 by Associate II
  • 2617 Views
  • 3 replies
  • 0 kudos

VIPER53DIP assambly Trace code

hello - need to know the assambly plant trace code for lot#  Label Trace codes : GF209402  what plant F stand for  can you please share decoder    

presto by Associate
  • 1071 Views
  • 1 replies
  • 0 kudos

Resolved! Viper53e hardware ?

I have a hardware question about the viper53e chip.  For VDD startup voltage, what is the correct voltage to guarantee the mosfet switching will start?  I have seen some examples where 11.5V was not enough, and curious to know what the is the best VD...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.