STEVAL-ISA147V3 source code
Hello,I would like to get the source code for STEVAL-ISA147V3 please help me.Thanks
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hello,I would like to get the source code for STEVAL-ISA147V3 please help me.Thanks
Hi all,I am designing a wearable device with wireless charging.I have consulted the STDES-WLC38WA solution for the receiver circuit.Now I want to buy STDES-WBC86WTX and STDES-WLC38WA (images in the attached) for testing first, but I found they are no...
Hello,We are designing in this part on a new board and I am trying to find out if the factory vanilla part is shipped with working firmware or not? I have not been able to find any definitive information on this. I would generally expect a part like ...
Hi, the STSPIN240 datasheet states that the absolute maximum ratings for logic input voltage should be between -0.3V and 5.5V. However, it is unclear whether the logic input voltage can exceed VS.Can the logic input voltage exceed VS?Thanks,
We have integrated the STWLC38 into our wireless power receiver design and are aiming to utilize the full 15W power capability. However, we have encountered an issue when using the latest QI2 (MPP) chargers. Our receiver remains in BPP (5W) mode, and...
Hi All, I'd love to add Wireless Charging to a project that is particularly space constrained!I've found the WC Receiver STWLC38 which ticks a lot of boxes, but requires a lot of external components. Has anybody used this successfully?What is the min...
Hi,I am designing 2.7kw boost converter for which I am using SCTW100N65G2AG MOSFET. In the datasheet it lacks information about switching times(like rise time fall time and delays) and max DV/DT the MOSFET can take before failing. I feel these data i...
Olá; Você pode me ajudar sobre esse Diodo? Código de marcação: GAB GP 108
Hi, I want to design AC-DC converter using VIPER26H. The suitable development board is STEVAL-ISA081V1 which is based on VIPER26L. Can someone help me to find a transformer manufacturing part no.? I want 12V 10W output.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.