Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DC-DC converter

Hi,In one of my applications, I require to design isolated DC-DC converter with following features:Input: 24V (Nominal)Output: 0-150V adjustable by a controller (With the help of reference voltage)Power: 70WI've tried some designs that's generated by...

STEL12H24PUR

HiCan I ask you if is possible, using STEL12H24 eFUSE, to implement the reverse polarity protection using small components?We need to redesign an old project and We need of this feature, but we have a tiny area on the PCBCan you suggest to us other p...

PaoloZ by Associate
  • 688 Views
  • 1 replies
  • 0 kudos

Using AET-MOT-2DC70s1

Hi, not sure if this is the right section, but: I have been given an AET-MOT-2DC70S1 motor controller board (https://www.st.com/en/evaluation-tools/aek-mot-2dc70s1.html#overview) and I'm trying to work out how to get it going. Starting simple trying ...

Piran by Associate
  • 693 Views
  • 0 replies
  • 0 kudos

Find IC

Hello, I am Chintan Mevada. I am an Embedded Hardware Design Trainee. I have Find IC that specification have Battery Management I²C controlled, 1-4-cell, 5-A buck-boost solar battery charger with dual-input selector and MPPT.

Chintan2 by Associate
  • 1323 Views
  • 1 replies
  • 0 kudos

GaN based half bridge board with gate driver

Hello,I am looking for GaN based half bridges or full bridges evaluation board with gate driver for 250-400V and 3.3kW power rating for Dual active bridge DC-DC converter.Kindly suggest evaluation/ development board for the same Thanks & RegardsAbhis...

Stacking TVS Diodes onto Resistors for Space Saving

Hello we have a need to string the SMAJ58A-TR TVS Diodes with some chip resistors in parallel and I'm wondering if we could physically stack the diodes on top of the resistors due to limited board space. If so, what resistor package would be ideal an...

BTA26-80BWRG

Hello, I have questions about a project we developed a long time ago. I will put the schematic below. We are using the BTA26-800BWRG (U8 and U9) in the schematic to parallel two inductors. The voltage applied to these two inductors is an ultrasonic s...

Joe26_0-1738256270041.png
Joe26 by Associate II
  • 4797 Views
  • 15 replies
  • 0 kudos

viper22a short circuit protection problem

Hello, I use viper22A for 220VAC to 14VDC-1A PSU. When I shorted output, around 3A current flows from Ampermeter. Viper22A datasheet explain that if output is short circuit no feedback will come from optocoupler, FB pin voltage will be 0V (my measure...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.