Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STPMIC25APQR LDO Programming Issue

Hello We are currently working on programming the STPMIC25APQR Power Management IC and are facing some issues related to the LDOs.As per the datasheet, there are no NVM control registers for LDO1 and LDO4, with their default output voltages specified...

Aks by Associate III
  • 958 Views
  • 1 replies
  • 0 kudos

Resolved! L9396 VBST overvoltage

Hi team, I have a question about L9396 VBST and VB voltage. The normal operation voltage rage of VBST and VB pin is (-0.1V,19V), and the absolute maxmum ratings of VBST and VB pin is  (-0.3V,40V). So, in case that the voltage is (19V, 40V), what will...

PAULZHAO by Associate
  • 1547 Views
  • 3 replies
  • 0 kudos

Resolved! BTA40-600B, optocoupler and snubber

I intend to design a microcontroller circuit with a BTA40-600B RD91 to control the power delivered to a heating resistor (220Vrms, 12Ω, 4KW). I thought about using the MOC3023 to mediate the activation of the BTA40, but I don't know if it is the most...

C source code for STSW-3KWTLCP

Hello and nice dayI am looking for STSW-3KWTLCP source code.As you know, the .bin and .out files are uploaded on the product page, these files are definitely obtained from the codes which written in C language, I would like to know how I can access t...

Hamez by Associate II
  • 2146 Views
  • 5 replies
  • 2 kudos

Resolved! LDO29300P2MTR

We have implemented the following circuit. This matches the application circuit given in datasheet of LDO29300P2MTR.But it does not yield expected output. We need help!!

IMG20250328160749.jpg
saran by Associate III
  • 4414 Views
  • 13 replies
  • 4 kudos

WLC38 - compatible chargers

Hi,We are developing a product using the WLC38 as RX.It works OK in combination with wbc2tx50 board, and a single Spigen QI charger we found (no overheating, constant power > 10W achievable).However using any other charging pads (either Qi1 15W or Qi...

mohimm by Associate
  • 947 Views
  • 1 replies
  • 0 kudos

L99DZ100G Out1 to Out6 remains High by default.

I am working on L99DZ100G IC. I am able to communicate with L99DZ100G correctly. But when I check Out1 to Out6 , I am getting 12V by default. If I make on and off CR4.B.OUT1_HS and CR4.B.OUT1_LS respectively it is working correctly. If I make off CR4...

prat by Associate
  • 1151 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.