Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6470: max acceleration register too low

Posted on November 12, 2011 at 20:20Hello, we have been testing the L6470 and are quite pleased with it. Very simple to use IC.But for fast movements the max acceleration value of 59.590 step/s2 is just too low.Small stepper motors (1.5 Amp) can eas...

L6470 dynamic speed adjustment

Posted on October 05, 2011 at 14:24Dear all Im' working with the L6470 using MOVE commands. Now I have a question about speed adjustment on-the-fly. It seems not possible to change speed during a move command is under execution. I really need this ...

flavio2 by Associate II
  • 1677 Views
  • 3 replies
  • 0 kudos

BLDC motor control

Posted on October 03, 2011 at 01:19hi, I am going to use Allegro 4931 3-phase motor pre-driver for my Brushless DC motor control project. Now I need a microcontroller to control the Allegro4931. Can anyone recommend me the best chip I can use for it...

ncarthic by Associate
  • 1528 Views
  • 3 replies
  • 0 kudos

Viper53 24V-1A full range

Posted on September 22, 2011 at 17:08 Hi I have one new project for my application and I have used the Viper53-E (dip8) to build a small SMPS AC/DC. After the selection of components with the VIPER SOFTWARE, I have build the SMPS, but don't have t...

L6207

Posted on September 07, 2011 at 10:11Hi gentlemen I'm planning to use L6207 PD for 2 brushed D.C motors, does any body know whether is it possible to use n.c. pins close the outputs to increase the path's width or they must be left unconnected. I'm ...

apoggiali by Associate II
  • 1224 Views
  • 2 replies
  • 0 kudos

Brushless dc motor animation

Posted on September 06, 2011 at 13:15to easily understand how a brushless dc motor works according to hall and phase signals.http://player.vimeo.com/video/28655973?title=0&byline=0&portrait=0

Stm32 Encoder interface

Posted on July 12, 2011 at 09:44Nid help in Stm32 Encoder Interface, to turn the motor in clockwise and anti-clockwise direction. Thanks 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.