Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stepper motor controller with L6506 and L298

Posted on October 01, 2012 at 11:52Hi, I'm new to this forum, because I really need some help designing a driver board for a stepper motor. The motor has to phases, 1A per phase, 8.6V and will be controlled over A+/- and B+/- (bipolar). The board wi...

giamnac by Associate
  • 1564 Views
  • 2 replies
  • 0 kudos

LED2000 vs ST1CC40

Posted on February 23, 2013 at 12:58Is there any difference betweem ST1CC40 and LED2000 regulators?I coundn't tell any difference based on datasheet info.

rnd2399 by Associate
  • 1271 Views
  • 2 replies
  • 0 kudos

LED2000 circuit parameter measurement

Posted on February 21, 2013 at 12:35I have built up a prototype board of a 2A white LED driver using the LED2000 step down converter with a single LiIon battery as the power source. Everything seems to be working as it should, but I would like to te...

L6470 & Maximum currect limiting

Posted on February 28, 2013 at 11:20Hi, I'm evaluating the L6470 for a project. Going over the datasheet I noticed that the minimum value for 'maximum current limiting' is 375mA. I need to drive a very small stepper (6mm) with 12V power source. Acco...

Frequency pwm with stm3210b

Posted on December 05, 2012 at 10:23Hello, I'm working with stm3210b-eval, I'm doing the following procedures : 1 : I generate with st Workench files in systems drives and params 2 : I compile with IAR But, in ST workench, the frequency params is 16...

PID controller

Posted on January 30, 2013 at 19:06I want to use the pid function in the library arm math. if I project  the PID controller in the domain S as I can find the constants KI, KP, and KD in the discrete-time to give the PID controller?thanks for your he...

fullcaos by Associate II
  • 1508 Views
  • 0 replies
  • 0 kudos

STM32F4

Posted on January 08, 2013 at 15:24Hi, I am using the STM3240G card with STM32F4 microcontrolleur. I would generate PWM for motor control. However, I need to handle data coming from a primary card ( beagle board) by ethernet (RJ45) with udp protocol...

IFN003V1, MC Library v3.0, 3.2, IFN003V1 Patch

Posted on January 11, 2013 at 18:38I'm attempting to get started with an IFN003V1 board.I am new to STMicro software tools and eval boards.I could not find V3.0 of the MC Library, so I installed V3.2.  I didn't find an IFN003V1 project, so I attempt...

jack2399 by Associate
  • 1226 Views
  • 3 replies
  • 0 kudos

L6470 problem: continuously read out status register

Posted on December 21, 2012 at 16:16Hi, I�m playing around with the L6470 which finally worked quite well. But now I�m experiencing the following issue: I want to continuously monitor the status register of the L6470. But when I send a �run� command...

post by Associate
  • 764 Views
  • 1 replies
  • 0 kudos

L6470 vibration

Posted on November 16, 2012 at 22:38Hello! My question is in follows:I got L6470 working, but not in a desirable way. Stepper motor vibrates in all speed range. It seems that phase current form distorted as shown in Fig. 15 (Section 7.3, p. 35 of da...

srg0016 by Associate II
  • 1704 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.