Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Phase controlled Rectifier

Posted on July 19, 2013 at 05:44How to Control the SCR with Microcontroller. I dont want to mix the Digital Signal Ground with the High Voltage Ground. But the SCR will need the Gate current in uA w.r.t its Cathode. But I couldnot connect the Cathod...

0690X00000605ZkQAI.png
saraaj100 by Associate II
  • 1466 Views
  • 1 replies
  • 0 kudos

Triac triggering circuit with a positive power supply

Posted on December 01, 2016 at 00:27 After reading AN3168 I found a paragraph that I do not actually understand and seemed weird for me .  Page 8, ''With the bipolar solution, to keep the current sourced to the gate, the only way is then to use a PN...

Increase the Power capabilities of STEVAL-ILD004V1

Posted on October 12, 2015 at 20:29I need to support a 2-wire 500W dimmer instead of just a 300W dimmer at 110VAC 60Hz US. What are the power limiting components of the ST Dev Kit? The 2 1N5404 diodes are only rated for 3A which would be 360W. Is th...

LD39130SPUR Adj resistor values

Posted on November 30, 2016 at 23:34What is the formula for Vo vs ADJ? Or in other words, how should R1 and R2 be chosen to get a specific output voltage?The data sheet, DocID025199 Rev 2, does not appear to include the necessary formula or ratio.

L99SD01

Posted on January 26, 2016 at 15:16Has anyone been able to read the fault register. I have no problem reading back set-up, but fault is hidden.  RichA #l99sd01

LED Power Supply

Posted on November 22, 2016 at 05:42Can anybody suggest me reference design for driving LEDs array along with micro controller.Here is my requirement :- Output 1 :- 17V, 400mA (Constant Current)Output 2 :- 3.3V, 1A (Constant Voltage)Power :- 12WIs...

anuj by Associate II
  • 714 Views
  • 0 replies
  • 0 kudos

HVLED815PF spice model or Excel files

Posted on November 14, 2016 at 19:08Hi There,We would like to design a Wide Mains, HPF, PSR, CV 25V 11W power supply using the HVLED815PF, however the eDesignSuite only allows to use it as a LED driver (constant current). There is an application not...

ppereira by Associate II
  • 707 Views
  • 0 replies
  • 0 kudos

Why VNH3SP30 overheat by upper 1KHz PWM Frequency?

Posted on November 07, 2016 at 21:21I bought VNH3SP30 a few years ago and recently used them in my self design board.I want to drive it by 3~5 KHz PWM freq. based on its spec. (Up to 10KHz as mentioned in its Datasheet). but when apply upper 1KHz PW...

mohsen2 by Associate
  • 669 Views
  • 0 replies
  • 0 kudos

SENSORLESS BLDC DRIVERS L6234 & L6235 + ANALOG

Posted on November 07, 2016 at 20:45Hello,Appreciate for any assistance concerning the two bldc drivers as bellow:1. Can L6234 and L6235 be use to drive a Sensorless BLDC Motors?2. Can the L6234 AND L6235 accept an analog reading - kind of vin throu...

barg6813 by Associate
  • 840 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.