Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use STPM33/34?

Posted on January 12, 2018 at 10:32Hi All;   I would like to use STPM33/34. How can I use it?. And Where is an example?#current-measurement #stpm33 #stpm34 #stpm3x

Gz by Senior
  • 922 Views
  • 0 replies
  • 0 kudos

VNH5019 Thermal Issues above 20A

Posted on December 02, 2017 at 02:25Hi,I've got some problems in getting the max Current capability of 30A out of the Chip. As soon as the Current goes above 20A the Chip will sooner or later switch of Halfbridge B. I think the problem is to get the...

STM8 problems by setting duty cycle

Posted on January 09, 2018 at 09:38Hello community,i got a problem when i want to create on my stm8 eval board a pwm signal with 350khz and variable duty cycle from 0-100.i calculate the the values for the registers as follows:PWM Frequency = Clock ...

X-CUBE-SPN7, 6Step_Lib.c

Posted on January 06, 2018 at 01:24Three questions regarding MC_SixStep_Ramp_Motor_calc()1.) What unit do the mechanical acceleration rate parameters/variables have? (apparently not 1/min/s or rad/s²)2.) 'mech_accel_hz = SIXSTEP_parameters.ACCEL * ...

Jakob K. by Associate II
  • 967 Views
  • 0 replies
  • 0 kudos

What is the main-chip of ''STEVAL-SPIN3202''?

Posted on December 18, 2017 at 03:40 I brought a 'STEVAL-SPIN3202'. It based 'STSPIN32F0A'.But main-chip written as follows.-----------------------------------------SPIN32F0FN02U A5THA 11 722ST @ A-----------------------------------------Is this 'ST...

Motor doesn't start with encoder

Posted on June 24, 2017 at 22:25I'm using the SPIN3201 eval board and have had it working in sensor-less and Hall modes, but i'm looking for better low very low speed, < 10 rpm behaviour where the halls don't produce smooth torque. I've attached a 1...

STC3117 Error in Application Note

Posted on October 31, 2017 at 01:26There seems to be an error in either the datasheet or the applicatio note of the STC3117 gas gauge.The error is in the bit description of the REG_MODE register, specifically the VMODE bit. The datasheet says the fo...

0690X00000608ntQAA.png 0690X00000608oIQAQ.png 0690X00000608fCQAQ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.