Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6480H Stall Detection - Does It Really Work?

I'm trying to evaluate if the L6480H stall detection actually works. We have been using the L6470H and we proved that stall detection with that chip did NOT work properly.I bought the EVAL6480H and STEVAL-PC0009V2 boards with the hope that I could pr...

L4970a Output Oscillates

Posted on March 04, 2014 at 09:46I need the following: 24V vehicle input. Allow for 28V. 13.8V @ 10A output. I used an L4970a. My circuit delivers the load, no problem.On initial switch on with no load, the output is stable. When I place a load up t...

adco by Associate
  • 889 Views
  • 1 replies
  • 0 kudos

RHFL4913A datasheet short circuit current vs. Rsh

Section 7 Typical Characteristics of the RHFL4913A datasheet contains Figure 44 and Figure 45. These figures state the output voltages used to generate the plots but don't mention the input voltage value. Can we assume that the input voltage is 2.5V ...

PHo by Associate
  • 800 Views
  • 0 replies
  • 0 kudos

How to reconfigure STEVAL-ESC001V1 to hall inputs

The gui allows reconfiguring to HALL inputs, which is why we purchased these boards. To test some motors during fast startup using hall sensors.When setting up HALL inputs there appears to be no valid pin configuration to get the sensors connected. D...

kyrreaa by Associate III
  • 876 Views
  • 1 replies
  • 1 kudos

L9826 - In SPI communication what should be the CPOL & CPHA setting of Master Micro controller for the proper communication with Slave L9826.

 In the datasheet it is mentioned as "The 8-bit command data are transmitted into L9826 shift registers every CLK falling edge". So which means the master uC sends out the data for every falling edge of the clock and the Slave L9826 samples this data...

Rajmohan by Associate
  • 1258 Views
  • 0 replies
  • 0 kudos

Viper37LD - does not regulate output voltages

I'm using Viper37LD in my project with the following features:Vin: 85-270VACOut1: 12V-1.5AOut2: 15V 0.125mAI used eDesignSuite to calculate component values.I have some boards mounted and I have the following situations:1- The source does not regulat...

JunexR8 by Associate II
  • 906 Views
  • 0 replies
  • 0 kudos

Viper37LD - does not regulate output voltages

I'm using Viper37LD in my project with the following features:Vin: 85-270VACOut1: 12V-1.5AOut2: 15V 0.125mAI used eDesignSuite to calculate component values.I have some boards mounted and I have the following situations:1- The source does not regulat...

JunexR8 by Associate II
  • 1013 Views
  • 0 replies
  • 0 kudos

STEVAL-PCC009V2 + EVAL6480H with cSpin and minimum wait time between sending the cSPIN_Set_Param() command (IAR C/C++ IDE)

Dear all,after some time I'll be able to correctly run the demo applications that came with the cSpin firmware libraries (search about STSW-SPIN005 on the ST site).The first part of this post is about how to set the demo design and compile it, the la...

FF1 by Associate III
  • 1099 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.