Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Always get STUSB4500 Not Detected message when using NVM GUI

I have checked and re-checked this. Also used another USB to I2C converter and can read the registers just fine. Put an I2C analyzer on the setup and I see no activity when the GUI program starts.Today on Github I found a HwCheckUtility.exe file. It ...

0690X000006DMH6QAO.png
jwhit.10 by Associate II
  • 4041 Views
  • 8 replies
  • 0 kudos

Resolved! two different IPS160H pinouts found

I am using IPS160H switch as a power switch input to DC/DC converters. But now I am confused to see a discrepancy between the data sheet and the STEVAL-IFP028V1 evaluation board schematics how to power the chip (Vcc). a) In IPS160H datasheet it says ...

0690X0000087pSHQAY.png 0690X0000087pSlQAI.png

ISSUE in en.x-cube-spn3 code

Hey,I note That There is an instruction ERROR in en.x-cube-spn3 code.in Powerstep01_SetDeviceParamsToGivenValues(uint8_t deviceId, powerstep01_Init_u_t *initPrm); function of powerstep01.c file, at line 1912 to 1914, the instruction, " Powerstep01_Cm...

Changing the MOSFET on X-NUCLEO-IHM08M1 to STP110N7F6.

Dear All,​I changed the MOSFETs on IHM08M1 to STP110N7F6 and modified the settings of dead time of Driver and Mosfet in MC work bench. But the BLDC can't run well(it doesn't reve-up often) . The manual of MC work bench only indicate user to modify mo...

AChen.17 by Associate
  • 919 Views
  • 1 replies
  • 0 kudos

I am working with VN5E050MJ-E what are the common fail modes?

The VN5E050MJ-E is used as a over current protections devices. We monitor the current via the current mirror output and disable the device when the current reaches the preset threshold. The threshold is well below the max rated current of the devic...

JCarr.13 by Associate
  • 679 Views
  • 0 replies
  • 0 kudos

Is the SPV 1040 suitable for using multiple PV cells in parallel? And how can increase the efficiency for Li-io charging?

HeySo I'm currently building a Solar charger for a 10000mAh Li-Io battery pack and I came across the SPV1040.For the project the charge current does not have to be high so the batterys are just slowly charging but I wanted to use Solar panels with ab...

PFran.19 by Associate
  • 974 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.