Hello community, Question is related to application note no. 308
Please help to use two anti-parallel SCRs in place of a single triac ? Regards and thanks in advance.
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Please help to use two anti-parallel SCRs in place of a single triac ? Regards and thanks in advance.
Hi all,I am using F303re to control an e-bike motor. I use GPIO PA6 connected to a speed sensor located on the wheel of e-bike.Every time the wheel takes a loop, an interrupt is sent from the speed sensor. Below is GPIO setting: GPIO_InitStruct.Pin =...
Hi. Have an open support ticket on this request but so far no reply so perhaps staff is on vacation. We are considering the ST devices for a pending product roadmap.Can the STWBC-MC kit be used for charging portable devices (watches, fit bands, etc.)...
I wish to use two anti-parallel SCRs for controlling a transformer with specifications of Pri:220V, Sec:7V, at 3500 amps. Is it possible ? What changes , if any, are required in the circuit ? Please help.Regards.
Hi everyone, i bought STEVAL-ISA147V3 to understand well D-SMPS. At first try, i didn't connect fan to output load, so the fuse blow and some diodes at PFC circuit (D9, D12 and D13) become short-circuit . Then, i realized i should connect load to out...
HiWhich registers can be read/write on the STUSB4500? What are the register addresses?The datasheet only mentions the NVM parameters and their default values, how do you set them via i2c?ThanksJM
Configurations are as followI am using default OCV table and 660mAh battery (4.2v max) with <70 mOhm internal impedancefirst OCV value = 7788REG_CTRLvBattTWI_Write(1, BATT_GAUGE_ADD, REG_CTRL, 0x02);REG_MODEvBattTWI_Write(1, BATT_GAUGE_ADD, REG_MODE,...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.