Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I use FOC+Hall method and I have a problem with startup.When I start the motor, the motor has startup vibration.I try to adjust speed/IQ/ID Kp, Ki to make the startup stably.But it still has startup vibration.any suggestion for this kind of problem?T...
Would you please offer me the Q&A report of L6472PD? I want to get the MTBF data of this IC.
I want to control position using STEVE-SPIN3204.BLDC 24V motor and external encoder were used and it was set as position controller. I compiled and downloaded it, and when I start the motor, the motor vibrates.The way I know 1) motor start 2) Move th...
Our circuit uses an L99MC6 6-ch driver in 3-ch bridged mode to drive 3 relays (Song Chuan p/n 301-1A-C-R1-U03-12VDC) with a common +12V rail connected to the relays. The relays are activated by a sink output. The circuit's 3.3V logic Vcc is temporari...
I don't know if this is the correct place to ask this question.In 'AN2450 LLC resonant half-bridge converter design guideline', it gives many equations. But I can't figure out how to get the Equation 45, particularly the section after ">=".Anyone can...
Dear All,I've a problem with my step-down regulator L7985A.On power up, the DC / DC is activated when the ENABLE pin reaches about 880mV, while on the datashhet it is reported 1.2V as the ON threshold.Can you explain to me what this difference is due...
I want to search datasheet about '92E540'. But I couldn't found that. Can I get the datasheet about IC '92E540'?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.