Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hi, I cannot find in the datasheet whether the base of the STBR6012 is electrically isolated, and if so what the isolation voltage is.Thanks!
Set up > Config: default (reg0 ~ reg19) > Latch: by SYN and SCS pin > Interface: uart > Reading interval: 5sLogCall emberAfPluginPowerMeterIcReadEventHandleruUART0_SSB_TX_Buffer[0]:48uUART0_SSB_TX_Buffer[1]:FFuUART0_SSB_TX_Buffer[2]:00uUART0_SSB_TX_B...
I would like more information about the LD1117DT18TR PBF marked:ST (e3) GN L1117 18GKOW7347ST is the logo of the manufacturer STMicroelectronics. Is the LD1117DT18TR PBF the original product of your company? Please decipher the release date (...
Я хотел бы получить дополнительную информацию о маркировке LD1117DT18TR PBF:ST (e3) GN L1117 18GKOW7347ST - �?то логотип производител�? STMicroelectronics. Явл�?ет�?�? ли LD1117DT18TR PBF оригинальным продуктом вашей компании? Пожалуй�?та, ра�?ш...
Hello, i'm here to ask you becouse i not understand how improve (if possible) the time spees in PiL mode. i've build my FOC+Space Vector compute model on simulink (there are sin, cos functions for Park Transforms ) with fixed step size of 1us, and 1....
Hello,has the VNH7070AS an active freewheeling mode implemented?best regards
As shown in my picture, I have connected both 3.3v to both the board and the uart pins and veried that it is providing 3.3v. Is this the correct connection? Should I be expecting something from the uart pins? I haven't done any configurations yet.
How much is the max load current capacity for every load output of the STEVAL-GLA001V1 evaluation board?Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.