Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hello,I got this board and connected power and could not see any activity on the ST-LINK USB port (J11). I installed the drivers and used 115200,8,N,1, no flow control. There's no startup message or response to CR or serial echo.I can connect to the ...
Hi!The company I work for have a product that uses the LDLN025 LDO regulator. The LDO drives an SIGFOX module, a couple of pullup resistors that goes to a always-powered uC and to a ST25DV64K IC. All of them has 100nF decoupling capacitors + a 22uF o...
FERD20L60C, Using this product in a simple 3ph rectifier and find that the diodes show conduction in both directions using a commercial quality DMM, Behave as one would expect using a higher quality meter, why?Using two inexpensive, but not junk DMM...
I want to interface 433MHZ rf receiver to use rf remote with stspin32f0 for speed control.I am using external gpio interrupt and microseconds TIM3 interrupt to decode received remote codes from rf receiver.I tested above setup without motor attach to...
Alternatively single phase inverters will also work. Only power board with gate drivers and switch protection is needed. around 300Vdc link 5KW is sufficient.
Hello,is it just me or is the software just not working at all?Using a pretty new Windows 10 machine and trying to connect the STSW-STWBCGUI Graphical user interface Version 3.48 to the development boards STEVAL-ISB027V1 and STEVAL-ISB045V1.Doesnt se...
I have been able to compile and load the X-CUBE-SPN5 example to my NUCLEO-F401 with an IHM05A1 board. I notice in the example folders that there is a BSP folder with L6208 component and MotorControl folders. How can I make these folders/drivers acces...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.