Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What is the L6474 ABS_POS register really reporting?

I am looking at using the L6474 to drive a stepper motor. I have a question about the absolute position register (ABS_POS).It says it is the current motor absolute position, but I want to clarify that it really is just a counter for the number of ste...

DSabo by Associate III
  • 1040 Views
  • 2 replies
  • 0 kudos

X-Nucleo-IHM02A1 & STM32 Nucleo F302R8 error code

Bonjour, je suis en train de travailler sur un projet dans lequelle je dois commander deux moteurs pas à pas, j'ai acheté le driver IHM02A1 et la carte Nucleo-F302R8 .j'ai suivi toutes les étapes disponibles dans le guide de démarrage disponible par ...

k.B.8 by Associate
  • 820 Views
  • 1 replies
  • 0 kudos

Reverse Power flow for LD39050 regulator, what will it affect

Hello everyone,I have a question, and i hope someone can help me,I am currently building a circuit which contains 2 source of power;1- main source (3V CR2 battery)2- auxiliary source (5V USB in case of emergency)taking into consideration that all the...

ATare.1 by Associate
  • 826 Views
  • 1 replies
  • 0 kudos

Resolved! Steval -SPIN3201

Can I connect oscillograph to Steval -SPIN3201 for measurement currents of the phase? Where is this point on board?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.