Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi All, Sample code for L9600 IC to control H bridge

In one of my projects, I am using L9600 IC to control motor speed and direction. I followed all the steps which are mentioned in IC user manual, But No Luck. I am always getting H bridge status is disabled. Could you please provide steps or sample c...

HMach.1 by Associate
  • 1734 Views
  • 3 replies
  • 0 kudos

Led2001

Hi.LED2001 driver is chosen for my design.The eDesignSuite tool was used for my design.My goal is to use the LED with Vf of 3.0V and If of 3.0A.And, The input voltage of LED driver range from 3.5 voltage to 4.2V.The voltage across the feedback resis...

HKIM.21 by Associate
  • 2061 Views
  • 3 replies
  • 0 kudos

I am currently working on the gate driver system, I am a bit confused about the driving power and current requirements for IGBT driving. Are there any recommendations to the power supply required for a full 3-phase inverter? I am looking for 15V/-8V

I am working to create a 100KW 3-phase inverter to be used in an FSAE electric race car,I don't have much experience with bootstrapping and I am a bit confused about the driving power and current requirements for IGBT switching. Thanks.

JKran.1 by Associate
  • 1863 Views
  • 4 replies
  • 0 kudos

Resolved! P-Nucleo-IHM001 Motor Not rotating

I have ordered P-Nucleo-IHM001 via Digikey.When trying the default FW, both FOC and 6-steps, the motor is not rotating.I connected the motor to a drill and rotate it, all three wires will produce around 1V peak to peak.Here is the video when testing....

L6924D Reverse Polarity Protection Problem

My objective:I'm designing a charging station that need to charge 100+ single cell Li-Po battery together. L6924D fits all my requirements like it can specify the charging current, termination current and max charging time. ​My challenge:Since the ba...

VChew by Associate II
  • 1227 Views
  • 1 replies
  • 0 kudos

What is the PWM Ramp Voltage of SG3525

I need to calculate the analog compensator values so I need to know pwm ramp voltage of sg3525 but I cant find on datasheet, can somebody help me about it?

Cocal.1 by Associate II
  • 1380 Views
  • 1 replies
  • 0 kudos

Spice model (or model parameters) for STB6N60M2

I'm working on a hobby project half-bridge driver using the STB6N60M2. I estimated the tdon, tdoff, trise, tfall times based on https://www.vishay.com/docs/73217/an608a.pdf . From that, the STB6N60M2 gives me low losses for the power level I'm worki...

TMahb.1 by Associate
  • 808 Views
  • 0 replies
  • 0 kudos

VIPER012HS reset on 230VAC

Hi, I used the VIPER012HS controller following the non-isolated flyback scheme proposed by the tool design suit (which is the same by the datasheet) but after making the pcb I get a reset problem with the 230VAC mains voltage. I tried to input a dire...

PLi P.1 by Associate
  • 1355 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.