2021-05-20 5:37 AM
I am using a IHM01A1 Stepper motor shield with an STM32F401. The provided example for one motor from the X-CUBE-SPN1 package works as expected and I can properly control the motor.
Now I want to basically recreate the project from scratch as a prober STM32CubeIDE project with CubeMX/IOC files.
I spend literally hours for doing this, until everything combined properly as I was adding all the driver folders by hand and had to remove the drivers for all other boards except the F401RE (Linked folder in C-Project Options).
I have now an example which compiles and links without errors, but it doesn't run properly.
This is basically my main.c
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_TIM3_Init();
char *tmp_string = "Hello world\n";
BSP_MotorControl_SetNbDevices(BSP_MOTOR_CONTROL_BOARD_ID_L6474, 1);
BSP_MotorControl_Init(BSP_MOTOR_CONTROL_BOARD_ID_L6474, 0);
while (1)
{
HAL_UART_Transmit(&huart2, (uint8_t*) tmp_string, strlen(tmp_string), HAL_MAX_DELAY);
BSP_MotorControl_GoTo(0, 1000);
BSP_MotorControl_WaitWhileActive(0);
BSP_MotorControl_GoTo(0, -1000);
BSP_MotorControl_WaitWhileActive(0);
}
}I've traced the execution in the debugger. The code hangs within BSP_MotorControl_Init() and in there in the call to L6474_Board_Delay(1) - which does nothing more then HAL_Delay(1).
Funny enough I cannot step (F5) into L6474_Board_Delay() in the debugger.
And - when I do a HAL_Delay(1) BEFORE the call to BSP_MotorControl_Init(), this one works as expected and returns immediately.
This is my first try to setup a project with that shield so I might have done something fundamentally wrong (I basically added all necessary folders in the BSP subfolder of the SPN1 package to my project, added paths, etc.) as it seems I cannot add this extension via the IDE automatically.
I already verified that the clock settings are 1:1 between the examples.
What could be wrong. Project attached for your reference.
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.