In STPM34 Can we connect two shunt Resistors for measuring Current? If yes How?
I have Connected the two shunt resistor I am reading the current but when I connect one load another load current also updating.
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I have Connected the two shunt resistor I am reading the current but when I connect one load another load current also updating.
I am looking for documentation for the L9763 chip, SPI protocol. Do anyone have this? Or do anyone know where to download from?
Same issue as @PK.3 (but I would like the response to be shared with the community :beaming_face_with_smiling_eyes: ) : using a 4 volt OC 425 mA SC series photovoltaic, and SPV1040 with circuit matching STEVAL-ISV006V2 except Rs = 0 ohms and no VR4 (...
After a the device is charged the stwbc needs a power cycle before the it will come back in ping status. Is it possible to set the charger always into ping status after a charge is completed with the parameters?Thanks in advance, Marco
I'm building a sink only type PD device using a SAMD21G18A and the stusb1602, because the stusb4500 was not available so we changed our design. I have i2c communication with the device, and can read/write to the NVM (although I'm not sure I have the ...
Hello, I'm designing an AC switch with a TRIAC. This TRIAC is controlled by a phototriac. The following connexnio is used : R1 and C1 is a snubber to protect the phototriac. Is this case, is it necessary to add a second snubber (see below) to prote...
Hello, I am trying to use L6470 for stepper motor control.I tried to change L6470's step mode register from 0x07(reset value) to 0x05.But when I read it back after I sent a command, its value was the same.I use 6 L6470 chips but this problem happened...
Hi, I am looking AC Induction motor evaluation kit. I have worked experience with STM32F4 and STM32F7 series microcontroller. So i need to make AC Driver for AC Induction Motor with all Four Quadrant operation. So please suggest me the AC Inductio...
Hello all,I am trying to design a VFD using STGIF7CH60TS-L and stm32f030r8 micro.I found that ST has a motor control library for PMSM motors.But I could not find any reference to port it for induction motor.Could anyone please point me in the right d...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.