Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Control mechanism of VB_SW pin of L9396 component.

Hello,The component in question is L9396. I have a question about the properties of the 'Protected battery switch' pin (VB_SW) of this component. In the datasheet for this pin, both 'The device provides a fully protected switched battery output VB_SW...

AOZKA.1 by Associate
  • 926 Views
  • 0 replies
  • 0 kudos

STWLC68 OTP Programming in a automated production environment.

We've designed the STWLC68 in to our portable product. We've build low volumes of devices up to now with the STEVAL-ISB68GUI V1.4.1 up to now, but would like to ramp up our production and therefore requires to automate the process. Unfortunately does...

GBoth.2 by Associate
  • 779 Views
  • 0 replies
  • 0 kudos

Totem pole PFC Control loop designs

The page number 46 current control design, The DPWM gain is given as 10^-3. The PWM Timer max value is 1000 for 72kHz freq for a clock of 72MHz. Then 1000 means 100% duty, 500 means 50% Duty.. etc. So the per unit duty (0 to 1) Shall be multiplied wi...

AKUMA.5 by Associate
  • 1276 Views
  • 0 replies
  • 0 kudos

Detail STUSB4710 register map

Hi there ...Is there any document explain the STUSB4710 register map (in stusb4710.pdf)? I have already STUSB47xx_register_map_public.pdf, but nothing detailed!I'll appreciate for any help.With regardsJitu

JChou.1 by Associate III
  • 609 Views
  • 0 replies
  • 1 kudos

STEVAL-ISB68WA not working with standard Qi transmitters

"...it works out of the box when placed on a suitable wireless power transmitter." is what it says on page 1 of the user manual. I have several Qi compatible transmitter pads, and the STEVAL-ISB68WA does not power-up with any of them. (D3 does not ...

JDupr.2 by Associate
  • 1178 Views
  • 2 replies
  • 1 kudos

DATE CODE OF STB18NM80

Dear Sir/MadamI want to confrim the date code of a ST part STB18NM80,pls find attached label picture.Can you tell me if they're 20+ or 10+?I am confused.Pls help to check.Many thanks!Susan

SHuan.31 by Associate
  • 1537 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.