Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue with PWD13F60 driving dc brushed motor

I am using a EVALPWD13F60 and a stm32f103c8 bluepill to drive a small DC brushed motor. When duty cycle is above about 30%, the motor starts to oscillate. I couldn't figure what's wrong with my circuit and code. thanks.

0693W00000Y6yEBQAZ.jpg
DZhou.4 by Associate
  • 1237 Views
  • 1 replies
  • 0 kudos

I would like to know STM have 4 channel Isolated Gate driver?

Hi,I'm new and designing a DCDC converter. I'm looking for a 4 channel Isolated gate driver for full bridge. I'm able to find only single or two channel/half bridge Isolated gate driver. I cant find 4 channel / full bridge isolated gate driver in a s...

ARose.5 by Associate
  • 1635 Views
  • 3 replies
  • 0 kudos

First PCB: Power Delivery with STUSB4700

Hello Everybody,i would like to design my first PD Board using the STUSB4700 IC. Since i´m quite new to PD IC´s i thought it would be best practice to just follow the typical use case: "Power supply - buck topology" as seen in the datasheet. While re...

0693W00000Y7VxxQAF.png
DJunt.1 by Associate
  • 1117 Views
  • 0 replies
  • 0 kudos

TCPP01-M12 FLT fault indicator

I'd like to add an LED indicator to the FLT pin so it sinks current when it becomes active low. The LED anaode would be tide high with a resistor in series. The spec sheet says this pin has a resistance of 250Ohms when active. How much current can t...

RMas by Associate II
  • 1658 Views
  • 1 replies
  • 0 kudos

Resolved! Lifecycle of LDP01-47AY, D2PAK?

Dear Sir or Madam, could you please inform us about lifecycle of diode LDP01-47AY, D2PAK? Is this diode still in serial production?Thank you for your answer, Tomaz.

TPeli.1 by Associate
  • 1124 Views
  • 1 replies
  • 0 kudos

Resolved! Using the L6474 when Reading the Status Byte with the GetParam(0x20 + 0x19) and GetStatus() or Command(0xD0) I get different results for the Status Byte.

To be honest the difference is 0x7F03 for the ReadParam() and 0xFF03 for the GetStatus()The documentation L6474Data Sheet (DoclD022529 Rev 4) says Bits 13, 14, and 15 should be 1 all the time. In one case Bit 15 is always 0 and the other case Bit 1...

0693W00000Y6jqyQAB.png
KiptonM by Lead
  • 1348 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.