Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Connection of Vcc and Pvcc of STDRIVEG600

Hi there,​I am using the STDRIVEG600 to drive FETs for my application. However, I came across some confusion.​Would you please clarify the following question:​Are the VCC (pin 4) and PVCC (pin 5) internally connected as the attached picture with blue...

NK.5 by Associate
  • 1968 Views
  • 1 replies
  • 0 kudos

Need help interfacing with L9305

As I could not find any interface/programming guides in the software documentation section i need help interfacing the L9305 IC via SPI. Also I have a few queries.1) In the SPI section, the MSB is R/W bit. But what does 1 mean Read or Write ? 2) What...

BNara.2 by Associate
  • 1434 Views
  • 0 replies
  • 0 kudos

Part Marking for 8-SOIC

Would like to know the exact part number for 8-SOIC with marking "38438" or "3843B"or"ST MZ205" or "ST MZ20S".Also attached the image for your reference

DVisa by Associate II
  • 2239 Views
  • 2 replies
  • 0 kudos

SPV1050 and solar panel current

Hello,I have a circuit with an SPV1050, the max Ibatt is 70mA, I'd like to know what happen if the solar panel can source more than 70mA, i.e 100mA. Is it a problem for the panel or for the chip (i.e temperature increase too much) ?Best regards,Ricc...

RStra by Associate III
  • 799 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.