Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STEVAL-PMIC1K1 and USBSTICK issue

Hello, we are testing the PMIC1 for a new design, so we bought a STEVAL-PMIC1K1 eval kit.However, after some testing with the GUI, the STEVAL-USBSTICK suddenly stopped working.It seems to be some kind of current drain that killed the device, because ...

PAkRad by Associate III
  • 2883 Views
  • 6 replies
  • 0 kudos

SW / FW for STEVAL-ILL015V2

Hi, I have the STEVAL-ILL015V2 board.When I put the board into operation, I can use the buttons to select a few LED patterns.Is the firmware of this demo version available for download?The board also has a USB port. Is there also a PC software with w...

RKloi.1 by Associate
  • 766 Views
  • 0 replies
  • 0 kudos

Battery Management Gas Gauge solution

HI,Need your suggestion if there is any BMS IC's (Gauge, Charger) available with advanced feature from ST. Is there any solution available without characterizing the battery (no learning cycle), and it can be usable by doing register settings and wit...

SPatt.2 by Associate
  • 705 Views
  • 0 replies
  • 0 kudos

Resolved! TIMER1 outputs in STEVAL-SPIN3201 not working

Hi all,I am working with the STEVAL-SPIN3201 development board for controlling a BLDC motor. This board is based in the STSPIN32F0 controller which integrates the STM32F031C6 MCU. I attach the system-in-package block diagram taken from the datasheet....

adromo95 by Associate II
  • 1654 Views
  • 3 replies
  • 0 kudos

STEVAL-ISV020V1: MPPT for 3 phase brushless dc turbines

Dear ST Community,I would like to use this device for energy harvesting from a 3 phase brushless dc turbines. The MPPT algorithm from this device is created for TEG and solar power, so I wonder it's possible to use this with brushless dc motor.Thank ...

Khoi Ly by Associate II
  • 804 Views
  • 0 replies
  • 0 kudos

Choosing a Transil for Triac Over voltage protection.

Hi team,I'm working on a 3 Phase (400Vrms) Power board control system. Regarding the over-voltage protection of the triac, AN1996 suggests to use Transil across Gate and A2 of the Triac. 1) When Choosing a Transil, the peak voltage of our system is 5...

Salman S by Associate
  • 1052 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.