2023-04-18 7:22 AM
I know I could take a meter and simply check but I don't have any spare parts easily accessible to make this quick measurement.
Solved! Go to Solution.
2023-04-18 1:34 PM
Welcome, @ESant.3, to the community!
If by thermal pad you mean pin 4 from the data sheet, figure 21, then this pin is connected to pin 2 (GND). You can also see this in the data sheet on page 1, where both pins are marked with "2", i.e. the same potential. ;)
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
2023-04-18 1:34 PM
Welcome, @ESant.3, to the community!
If by thermal pad you mean pin 4 from the data sheet, figure 21, then this pin is connected to pin 2 (GND). You can also see this in the data sheet on page 1, where both pins are marked with "2", i.e. the same potential. ;)
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
2023-04-18 2:02 PM
@Peter BENSCH Thank you for your response, but this is in conflict with a direct case/ticket I put in to ST Customer support. This was Customer Support response: "To answer the question about the thermal pad, if its not specifically called out as a "connection" in the datasheet, then its floating internally (as most are). I just double checked the L5150 and that is the case. In other words, its not electrically connected. However for best thermal considerations, it is a good rule of thumb for it to be soldered to a large thermal/copper plane on the PCB which is typically a ground, but again it’s not electrically connected or required."
Is ST asserting now that it is connected internally?
2023-04-18 2:10 PM
You refer to ticket # 00177888, right?
Well, for me the data sheet is crucial and the most important source of information. There, as I mentioned, the fourth pin is marked as pin 2, from which I conclude that pin 4 and pin 2 (GND) are connected.
If Customer Support claims otherwise, you'd best check it yourself, because I don't currently have an L5150BN to measure.
2023-04-18 3:36 PM
@Peter BENSCH Winner! Peter is right, L5150BN Pin 2 is internally connected to the thermal tab/pin/pad in the SOT-223 package. Had to lift a pin on a production assembly, but worth it to get the answer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.