Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Motor Control configuration for DRV8323 driver

Hello, I am working on BLDC motor driver. I am use STM32G431 as control unit with Motor Control Workbench and DRV8323RH gate driver. I have problem with getting the motor to spin, as soon i I start it, i am getting under voltage error. And see some o...

PX.2 by Associate
  • 2779 Views
  • 2 replies
  • 1 kudos

L9963E Fault-L pin.

hiI made a board with stm32l431 and L9963E.The voltage, current and temperature values have been read successfully.In addition, it was confirmed that it operates with settings such as UT, OT, OV, and UV.However, the Fault-L pin does not change to hig...

Jeonghun_0-1707351121705.png Jeonghun_1-1707351672368.png Jeonghun_2-1707351774042.png Jeonghun_3-1707351883042.png
Jeonghun by Associate
  • 1003 Views
  • 0 replies
  • 0 kudos

Resolved! STWBC86 FTP

Hello,   I recently designed a wireless transmitter utilizing STWBC86, however, I have encountered a boot issue due to an empty FTP memory. I have been searching for firmware and a GUI to upload the firmware into the FTP, but have not had any success...

YChan.2 by Associate
  • 2218 Views
  • 2 replies
  • 0 kudos

Resolved! BTA16 vs BTA20

Hi all,We have an application of an electric heating boiler using BTA16 triacs to commute resistive loads of 13A (rms). The max. temperature in the triacs is around 70ºC-80ºC.We are studying the option of using the BTA20 triac instead of the BTA16 on...

DaniES by Associate
  • 3473 Views
  • 1 replies
  • 0 kudos

Requirement of DC-DC converter

Hi ST team,   I have requirement of DC-DC converter as per below :- Input voltage range: 20V-30V/1ARequired dual output  +15V and -15V.Input voltage range:  20V-30V/1ARequired dual output +10V and -10V.Input voltage range : 20V-30V/1ARequired output ...

prakash1 by Associate
  • 1559 Views
  • 1 replies
  • 1 kudos

Resolved! Using a STWLC38 with an optional USB-C charging

I'm looking for a reference schematic where I can use the STWLC38 for Qi charging, but the Qi charging will be disabled when a USB-C is plugged in. I also need the USB-C Vbus to be isolated from the connector while the Qi charging is active. I'd real...

BPolinske_0-1706719449014.png
BPolinske by Associate II
  • 3289 Views
  • 5 replies
  • 1 kudos

individual LED driver

Hi frds,I've choose blue color led, that led works mention voltage & current, but my doubts is i choosed driver led driver for each LED, Which one is best ?, pls  suggest anyone....This part no'sLED2001PHLED2000DRST1CC40DR  

screenshot.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.