2023-04-24 12:24 AM
Hi ST experts,
Would like to know if ST has any recommendation on battery charging solution?
The battery pack requirement is 7.4V 2300mAH which is 2-cells construction.
The intention is to change from standalone battery charger IC to a smart charger solution whereby it can help to prolong the battery lifespan for example having trickle charging and battery health (SOC) to keep the battery charge to max 80% (this can be done by configurable through software or hardware) and depth of discharge to 50% or 25%
Appreciate with any suggestions which can meets above-mentioned requirements.
Thanks.
2023-04-24 5:53 PM
Sorry. There is no solution fitting the requirements.
Battery charger portfolio:
https://www.st.com/en/power-management/battery-chargers.html
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.