2021-04-13 5:06 AM
2021-05-06 3:19 AM
Hello,
The VND5E160AJ-E is a dual channel high side drive, so there are only two INPUT pins, and each of the INPUT controls the relevant OUTPUT. The other input pin, called CS_DIS, allows to disable the diagnostic feedback in case the device is used in parallel configuration (two or more devices in parallel, sharing the same sense resistor).
The device is reliable, considering it is automotive grade, AEC-Q100 qualified.
Best regards,
Luigi
2021-05-06 3:19 AM
Hello,
The VND5E160AJ-E is a dual channel high side drive, so there are only two INPUT pins, and each of the INPUT controls the relevant OUTPUT. The other input pin, called CS_DIS, allows to disable the diagnostic feedback in case the device is used in parallel configuration (two or more devices in parallel, sharing the same sense resistor).
The device is reliable, considering it is automotive grade, AEC-Q100 qualified.
Best regards,
Luigi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.