2019-08-20 11:55 AM
I know this is a dumb question, but I've googled it and can't get an explanation. What is the "debug" column in the MAP file?
Also, it's alarmingly big... using Keil is there a setting I should use to compile without whatever is taking up that space? I don't see the typical debug/release config settings.
Thanks for the help.
==============================================================================
Code (inc. data) RO Data RW Data ZI Data Debug
206256 18706 599208 7644 443828 3533745 Grand Totals
206256 18706 599208 1628 443828 3533745 ELF Image Totals (compressed)
206256 18706 599208 1628 0 0 ROM Totals
Solved! Go to Solution.
2019-08-20 1:06 PM
It's stuff allowing the debugger e.g. to relate memory positions to variables, program counter to lines in the source etc.
Don't be alarmed, it's doesn't occupy a single bit on the mcu, it's all on the PC in the .elf file.
JW
2019-08-20 1:06 PM
It's stuff allowing the debugger e.g. to relate memory positions to variables, program counter to lines in the source etc.
Don't be alarmed, it's doesn't occupy a single bit on the mcu, it's all on the PC in the .elf file.
JW
2019-08-20 1:22 PM
There is a "Debug Information" check box in the Output options pane.
2019-08-20 1:23 PM
Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.