2025-01-28 8:50 AM - edited 2025-01-29 9:05 AM
Hi Everyone,
I have some problems with DFU on Windows 10. I use WeAct BlackPill boards based on STM32F411 MCU. This board has BOOT0 button which allow to update firmware using STM32CubeProgrammer and DFU mode.
Majority of the boards can be programmed in DFU mode using STM32CubeProgrammer with no issue. Recently I got couple boards that acts very weird: those boards enters DFU mode just fine, detects by STM32CubeProgrammer and able to connect, but as soon I try to erase or program those boards - STM32CubeProgrammer says "Connection lost" and that is it. After that those boards enters into DFU mode, STM32CubeProgrammer able to read serial number, but any attempt to connect failed:
16:51:36 : STM32CubeProgrammer API v2.18.0 | Windows-64Bits
16:51:45 : UR connection mode is defined with the HWrst reset mode
16:51:45 : USB speed : Full Speed (12MBit/s)
16:51:45 : Manuf. ID : STMicroelectronics
16:51:45 : Product ID : STM32 BOOTLOADER
16:51:45 : SN : 337F33963134
16:51:45 : DFU protocol: 1.1
16:51:45 : Board : --
16:51:45 : Device ID : 0x0431
16:51:45 : UPLOADING OPTION BYTES DATA ...
16:51:45 : Bank : 0x00
16:51:45 : Address : 0x1fffc000
16:51:45 : Size : 16 Bytes
16:51:45 : UPLOADING ...
16:51:45 : Size : 1024 Bytes
16:51:45 : Address : 0x8000000
16:51:45 : Read progress:
16:51:45 : Error: Data read failed
16:51:45 : Warning: Connection to device 0x431 is lost
16:51:51 : Warning: Connection to device 0x431 is lost
16:52:00 : Disconnected from device.
16:52:00 : Disconnected from device.
If I use ST-Link to program those boards, I able to connect in DFU mode again... until I try to reprogram it. Then same problem with connection appears again.
I tried two different cables and three different laptops - same result.
But then I decided to try another PC with Windows 11 and it works! It works every single time on two different Windows 11 based laptops with no problems! STM32CubeProgrammer version is the same(2.18), so it is not that, it is something else. I wondering what it can be.
I really want this issue to be fixed, because I can't use those boards for my SmartPendant project to control CNC machines based on grblHAL controllers, since it will be impossible to update firmware under Windows 10, and even worse - attempt bricks device until it will be reprogrammed on Windows 11.
@Pavel A. wrote:> since it will be impossible to update firmware under Windows 10
Windows 11 works better than Win10. Sometimes newer is better. Support of Windows 10 will end in October anyway. Time to update!
I wondering why some people give advices that doesn't helps at all.Не зря СССР называли "страна советов"...
I make those devices and sell them to hobbyists like me who converting benchtop mills/lathes into CNC. They can use different OS and I have no control of it. I couldn't just say "Oh, you have a problem? Time to update!". Beside, I tried it on Windows. Will it have same problem on MacOS? On a Linux? I don't know. But what I do know there some problems with some of MCU, because some boards work and some don't. And those problems potentially can be fixed on STM32CubeProgrammer side since it works flawlessly on Windows 11.
And questions I want to be answered:
1) If it bug in MCU, does it affect anything beside DFU? Crushing CNC machine is not fun.
2) Will it be fixed in STM32CubeProgrammer?
P.S. I reposted it from there: https://community.st.com/t5/stm32-mcus-embedded-software/ocasional-dfu-problems-in-stm32cubeprogrammer-on-windows-10/m-p/765994/
since this is more appropriate section. You can delete original topic. <-- Threads merged
Solved! Go to Solution.
2025-01-30 7:25 AM - last edited on 2025-01-30 7:32 AM by Andrew Neil
Update: Connection doesn't work when I connect board directly to one of USB ports on laptop itself, but works if I connect it to dock station connected to the same laptop via USB-C. I also noticed that there different Verbosity Levels in STM32CubeProgrammer. I set it to 3, and when it doesn't work, this is what it shows:
08:41:54:866 : UR connection mode is defined with the HWrst reset mode
08:41:54:924 : DFU status = 0 : OK
08:41:54:925 : DFU state = 4 : dfuDNBUSY
08:41:54:925 : Status: 0, State: 4
08:41:54:925 : sending an abort request
08:41:54:925 : DFU status = 0 : OK
08:41:54:925 : DFU state = 2 : dfuIDLE
08:41:54:925 : setting the address pointer to address: 0x08000000
08:41:54:925 : DFU status = 0 : OK
08:41:54:925 : DFU state = 4 : dfuDNBUSY
08:41:54:926 : DFU status = 0 : OK
08:41:54:926 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:54:926 : Device Descriptor:
08:41:54:926 : |_bLength : 0x12
08:41:54:926 : |_bDescriptorType : 0x01
08:41:54:926 : |_bcdUSB : 0x0100
08:41:54:926 : |_bDeviceClass : 0x00
08:41:54:926 : |_bDeviceSubClass : 0x00
08:41:54:926 : |_bDeviceProtocol : 0x00
08:41:54:926 : |_bMaxPacketSize : 0x40
08:41:54:926 : |_idVendor : 0x0483
08:41:54:926 : |_idProduct : 0xdf11
08:41:54:927 : |_bcdDevice : 0x2200
08:41:54:927 : |_iManufacturer : 0x01
08:41:54:927 : |_iProduct : 0x02
08:41:54:927 : |_iSerialNumber : 0x03
08:41:54:927 : |_bNumConfigurations : 0x01
08:41:54:927 : Configuration Descriptor:
08:41:54:927 : |_bLength : 0x09
08:41:54:927 : |_bDescriptorType : 0x02
08:41:54:927 : |_wTotalLength : 0x36
08:41:54:927 : |_bNumInterfaces : 0x01
08:41:54:927 : |_bConfigurationValue : 0x01
08:41:54:927 : |_iConfiguration : 0x00
08:41:54:927 : |_bmAttributes : 0xc0
08:41:54:927 : |_bMaxPower : 0x32
08:41:54:927 : Interface Descriptor Alternate Settings: 0x00
08:41:54:927 : |_bLength : 0x09
08:41:54:927 : |_bDescriptorType : 0x04
08:41:54:927 : |_bInterfaceNumber : 0x00
08:41:54:928 : |_bAlternateSetting : 0x00
08:41:54:928 : |_bNumEndpoints : 0x00
08:41:54:928 : |_bInterfaceClass : 0xfe
08:41:54:928 : |_bInterfaceSubClass : 0x01
08:41:54:928 : |_bInterfaceProtocol : 0x02
08:41:54:928 : |_iInterface : 0x04
08:41:54:928 : Interface Descriptor Alternate Settings: 0x01
08:41:54:928 : |_bLength : 0x09
08:41:54:928 : |_bDescriptorType : 0x04
08:41:54:928 : |_bInterfaceNumber : 0x00
08:41:54:928 : |_bAlternateSetting : 0x01
08:41:54:928 : |_bNumEndpoints : 0x00
08:41:54:928 : |_bInterfaceClass : 0xfe
08:41:54:928 : |_bInterfaceSubClass : 0x01
08:41:54:928 : |_bInterfaceProtocol : 0x02
08:41:54:928 : |_iInterface : 0x05
08:41:54:928 : Interface Descriptor Alternate Settings: 0x02
08:41:54:928 : |_bLength : 0x09
08:41:54:929 : |_bDescriptorType : 0x04
08:41:54:929 : |_bInterfaceNumber : 0x00
08:41:54:929 : |_bAlternateSetting : 0x02
08:41:54:929 : |_bNumEndpoints : 0x00
08:41:54:929 : |_bInterfaceClass : 0xfe
08:41:54:929 : |_bInterfaceSubClass : 0x01
08:41:54:929 : |_bInterfaceProtocol : 0x02
08:41:54:929 : |_iInterface : 0x06
08:41:54:929 : Interface Descriptor Alternate Settings: 0x03
08:41:54:929 : |_bLength : 0x09
08:41:54:929 : |_bDescriptorType : 0x04
08:41:54:929 : |_bInterfaceNumber : 0x00
08:41:54:929 : |_bAlternateSetting : 0x03
08:41:54:929 : |_bNumEndpoints : 0x00
08:41:54:929 : |_bInterfaceClass : 0xfe
08:41:54:929 : |_bInterfaceSubClass : 0x01
08:41:54:929 : |_bInterfaceProtocol : 0x02
08:41:54:929 : |_iInterface : 0x07
08:41:54:930 : Functional Descriptor :
08:41:54:930 : |_bLength : 0x09
08:41:54:930 : |_bDescriptorType : 0x21
08:41:54:930 : |_bmAttributes : 0x0b
08:41:54:930 : |_wDetachTimeOut : 0xff
08:41:54:930 : |_wTransferSize : 0x0800
08:41:54:930 : |_bcdDFUVersion : 0x011a
08:41:54:930 : USB speed : Full Speed (12MBit/s)
08:41:54:930 : Manuf. ID : STMicroelectronics
08:41:54:930 : Product ID : STM32 BOOTLOADER
08:41:54:930 : SN : 337F33963134
08:41:54:930 : DFU protocol: 1.1
08:41:54:930 : Board : --
08:41:54:930 : Device ID : unknown
08:41:54:930 : DFU status = 0 : OK
08:41:54:930 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:54:930 : Status: 0, State: 5
08:41:54:930 : setting the address pointer to address: 0x08000000
08:41:54:930 : DFU status = 0 : OK
08:41:54:931 : DFU state = 4 : dfuDNBUSY
08:41:54:931 : DFU status = 0 : OK
08:41:54:931 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:54:931 : DFU status = 0 : OK
08:41:54:931 : DFU state = 9 : dfuUPLOAD-IDLE
08:41:54:931 : Status: 0, State: 9
08:41:54:931 : sending an abort request
08:41:54:931 : DFU status = 0 : OK
08:41:54:931 : DFU state = 2 : dfuIDLE
08:41:54:931 : setting the address pointer to address: 0x08000000
08:41:54:931 : DFU status = 0 : OK
08:41:54:931 : DFU state = 4 : dfuDNBUSY
08:41:54:931 : DFU status = 0 : OK
08:41:54:931 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:54:931 : DFU status = 0 : OK
08:41:54:931 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:54:931 : Status: 0, State: 5
08:41:54:931 : setting the address pointer to address: 0x1fffc008
08:41:54:931 : DFU status = 0 : OK
08:41:54:932 : DFU state = 4 : dfuDNBUSY
08:41:54:932 : DFU status = 0 : OK
08:41:54:932 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:54:932 : receiving packet nbr: 0
08:41:54:932 : DFU status = 0 : OK
08:41:54:932 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:54:932 : sending an abort request
08:41:54:932 : DFU status = 0 : OK
08:41:54:932 : DFU state = 2 : dfuIDLE
08:41:54:932 : UpLoading data
08:41:54:932 : DFU status = 0 : OK
08:41:54:932 : DFU state = 9 : dfuUPLOAD-IDLE
08:41:54:932 : Database: Config 0 is active.
08:41:54:932 : DFU status = 0 : OK
08:41:54:932 : DFU state = 9 : dfuUPLOAD-IDLE
08:41:54:932 : Status: 0, State: 9
08:41:54:932 : sending an abort request
08:41:54:932 : DFU status = 0 : OK
08:41:54:932 : DFU state = 2 : dfuIDLE
08:41:54:932 : setting the address pointer to address: 0x08000000
08:41:54:932 : DFU status = 0 : OK
08:41:54:932 : DFU state = 4 : dfuDNBUSY
08:41:54:933 : DFU status = 0 : OK
08:41:54:933 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:55:115 : DFU status = 0 : OK
08:41:55:115 : DFU state = 9 : dfuUPLOAD-IDLE
08:41:55:115 : Status: 0, State: 9
08:41:55:115 : sending an abort request
08:41:55:115 : DFU status = 0 : OK
08:41:55:115 : DFU state = 2 : dfuIDLE
08:41:55:115 : setting the address pointer to address: 0x08000000
08:41:55:115 : DFU status = 0 : OK
08:41:55:115 : DFU state = 4 : dfuDNBUSY
08:41:55:115 : DFU status = 0 : OK
08:41:55:115 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:55:115 : UPLOADING OPTION BYTES DATA ...
08:41:55:115 : Bank : 0x00
08:41:55:115 : Address : 0x1fffc000
08:41:55:115 : Size : 16 Bytes
08:41:55:115 : DFU status = 0 : OK
08:41:55:115 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:55:115 : Status: 0, State: 5
08:41:55:115 : setting the address pointer to address: 0x1fffc000
08:41:55:115 : DFU status = 0 : OK
08:41:55:115 : DFU state = 4 : dfuDNBUSY
08:41:55:115 : DFU status = 0 : OK
08:41:55:115 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:55:115 : receiving packet nbr: 0
08:41:55:115 : DFU status = 0 : OK
08:41:55:115 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:55:115 : sending an abort request
08:41:55:116 : DFU status = 0 : OK
08:41:55:116 : DFU state = 2 : dfuIDLE
08:41:55:116 : UpLoading data
08:41:55:116 : DFU status = 0 : OK
08:41:55:116 : DFU state = 9 : dfuUPLOAD-IDLE
08:41:55:116 : UPLOADING OPTION BYTES DATA ...
08:41:55:116 : Bank : 0x00
08:41:55:116 : Address : 0x1fffc000
08:41:55:116 : Size : 16 Bytes
08:41:55:116 : DFU status = 0 : OK
08:41:55:116 : DFU state = 9 : dfuUPLOAD-IDLE
08:41:55:116 : Status: 0, State: 9
08:41:55:116 : sending an abort request
08:41:55:116 : DFU status = 0 : OK
08:41:55:116 : DFU state = 2 : dfuIDLE
08:41:55:116 : setting the address pointer to address: 0x1fffc000
08:41:55:116 : DFU status = 0 : OK
08:41:55:116 : DFU state = 4 : dfuDNBUSY
08:41:55:116 : DFU status = 0 : OK
08:41:55:116 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:55:116 : receiving packet nbr: 0
08:41:55:116 : DFU status = 0 : OK
08:41:55:116 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:55:116 : sending an abort request
08:41:55:116 : DFU status = 0 : OK
08:41:55:116 : DFU state = 2 : dfuIDLE
08:41:55:116 : UpLoading data
08:41:55:116 : DFU status = 0 : OK
08:41:55:117 : DFU state = 9 : dfuUPLOAD-IDLE
08:41:55:117 : UPLOADING ...
08:41:55:117 : Size : 1024 Bytes
08:41:55:117 : Address : 0x8000000
08:41:55:117 : Read progress:
08:41:55:117 : DFU status = 0 : OK
08:41:55:117 : DFU state = 9 : dfuUPLOAD-IDLE
08:41:55:117 : Status: 0, State: 9
08:41:55:117 : sending an abort request
08:41:55:117 : DFU status = 0 : OK
08:41:55:117 : DFU state = 2 : dfuIDLE
08:41:55:117 : setting the address pointer to address: 0x08000000
08:41:55:117 : DFU status = 0 : OK
08:41:55:117 : DFU state = 4 : dfuDNBUSY
08:41:55:118 : DFU status = 0 : OK
08:41:55:118 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:55:118 : receiving packet nbr: 0
08:41:55:118 : DFU status = 0 : OK
08:41:55:118 : DFU state = 5 : dfuDNLOAD-IDLE
08:41:55:118 : sending an abort request
08:41:55:118 : DFU status = 0 : OK
08:41:55:118 : DFU state = 2 : dfuIDLE
08:41:55:118 : UpLoading data
08:41:55:119 : libusb control transfer error [-9] : LIBUSB_ERROR_PIPE
08:41:55:119 : Error: Data read failed
08:41:55:245 : Warning: Connection to device 0x431 is lost
08:42:00:459 : Warning: Connection to device 0x431 is lost
08:42:09:606 : Disconnected from device.
08:42:09:647 : Disconnected from device.
I probably should done it earlier. Search this error shows that I am not alone:
Error - libusb control transfer error [-9] : LIBUSB_ERROR_PIPE
STM32CubeProgrammer 2.14.0 firmware update error over USB in Windows 10 64 bit
STM32CubeProgrammer DFU instable
I highly doubt that everyone in those topics has fake MCUs. I assume ST will not resolve this issue.
@Andrew Neil wrote:It seems that @Shlapunov.Nicolai has the PCB design resources - so why not just put the SMT32 straight onto the PCB? Why the plug-in board at all?
It is an hobby project, it started with all off the shelf modules. Then I decided to make a board to make it smaller. Initial idea was to use BlackPill connected to the board which will allow to replace it if it will be damaged, but turns out that while round connectors smaller than regular squire ones, it still make device too thick. My board contains only two layers, BlackPill has more. I am not sure if it can be done in two layers. More layers - more expensive board. Then placement fees, other parts cost and with volume of 10-30 boards it just doesn't give any benefits for this hustle.
And even if I'll do all this, when something will go wrong, some ST Employee probably will say "LCSC and JLCPCB is Chinese companies, may be they sourced fake STM32s" :D
2025-04-14 7:59 AM
Hello,
ST resources are dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes work properly with the firmware we provide.
Thank you for your understanding.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.