2020-05-24 1:39 AM
I have existing working code which uses uart and some GPIO functions. Its main.h has,
#include "ll_common.h", #include "stm32h7xx_ll_gpio.h", #include "stm32h7xx_ll_usart.h"
and few more ll headers.
Now I need to add I2C functionality to the code. I go through the code given at
en.stm32cubeh7_v1-7-0\STM32Cube_FW_H7_V1.7.0\Projects\STM32H743I-EVAL\Examples\I2C\I2C_EEPROM_fast_mode_plus\MDK-ARM, as the code uses HAL drivers , I make the following changes,
#include "stm32h7xx_hal.h"
#include "stm32h7xx_nucleo.h (in example its stm32h743i_eval.h)
2. Add USE_HAL_DRIVER to compiler per-proceesor symbols(it already has USE_FULL_LL_DRIVER)
3. I add stm32h7xx_hal.h, stm32h7xx_nucleo.h,stm32h7xx_hal_conf.h, stm32h7xx_nucleo_conf.h, stm32h7xx_nucleo_errno.h, stm32h7xx_hal_i2c.h, stm32h7xx_hal_i2c.c to the project.
4. I also confirm that in stm32h7xx_hal_conf.h , #define HAL_MODULE_ENABLED and all other relevant modules are enabled.
Even with all these, I am getting compilation error like
.\STM32H745I_Nucleo_CM7\Exe\STM32H745I_Nucleo_CM7.axf: Error: L6218E: Undefined symbol HAL_EXTI_GetHandle (referred from stm32h7xx_nucleo.o).
.\STM32H745I_Nucleo_CM7\Exe\STM32H745I_Nucleo_CM7.axf: Error: L6218E: Undefined symbol HAL_EXTI_IRQHandler (referred from stm32h7xx_nucleo.o).
.\STM32H745I_Nucleo_CM7\Exe\STM32H745I_Nucleo_CM7.axf: Error: L6218E: Undefined symbol HAL_EXTI_RegisterCallback (referred from stm32h7xx_nucleo.o).
and many more.... basically compiler is not able able to see any HAL symbols.
KEil Version:5.26.2.0
What am I missing ?
Also I am using NUCLEO-H745ZI-Q, but keil does not support this board. Can this be a possible reason?
I tried all that I possibly could, I am stuck.
Any help is appreciated. Thanks in advance.
2020-05-24 7:02 AM
Ok, HEADER files describe interfaces, they don't typically contain the code required for linkage.
Need to add the library SOURCE files to get closure, ie
stm32h7xx_hal_exti.c
Try Keil 5.29
2020-05-24 7:47 AM
Thanks for such prompt reply. I did add stm32h7xx_hal_exti.c, but still same undefined HAL symbol errors are coming.
Do I have to add other files like these. How do I know which files , I have add. Is there any document stating, the the code flow among HAL files ?
I have gone through the HAL and LL driver document but I think , what am missing is the dependency among HAL files and their behavior when LL files are used along with HAL files.
2020-05-30 4:43 AM
Those errors mean that stm32h7xx_hal_exti.c is still not added/compiled/linked properly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.