2017-12-27 6:11 PM
Hello,
I am studying about STM32H7 using STM32H743 Nucleo-144 board with IAR.
So, I updated recently version of IAR such as ver.8.20.
When a downloading and debug, occur syntax error.
Error message is
=============================================================================
Fri Nov 03, 2017 16:39:50: IAR Embedded Workbench 8.20.1 (C:\Program Files (x86)\IAR Systems\EWARM8\arm\bin\armproc.dll) Fri Nov 03, 2017 16:39:50: C:\Program Files (x86)\IAR Systems\EWARM8\arm\config\debugger\ST\STM32H7xx.dmac(203,69): [syntax error, unexpected '{', expecting ')' or ','] Fri Nov 03, 2017 16:39:50: Loaded macro file: C:\Program Files (x86)\IAR Systems\EWARM8\arm\config\flashloader\ST\FlashSTM32H7xxx.mac Fri Nov 03, 2017 16:39:50: Connected to ST-Link/V2-1 [SWD mode 1800 kHz] [Access port: 0] Firmware V2.J29.S18 (Probe no: 57142829) Fri Nov 03, 2017 16:39:50: Initial reset was performed Fri Nov 03, 2017 16:39:50: 2784 bytes downloaded and verified (17.43 Kbytes/sec) Fri Nov 03, 2017 16:39:50: Loaded debugee: C:\Program Files (x86)\IAR Systems\EWARM8\arm\config\flashloader\ST\FlashSTM32H7xxx_CM7.out Fri Nov 03, 2017 16:39:50: Target reset Fri Nov 03, 2017 16:43:56: HardFault exception. Fri Nov 03, 2017 16:43:56: The processor has escalated a configurable-priority exception to HardFault. Fri Nov 03, 2017 16:43:56: An imprecise data access error has occurred. Fri Nov 03, 2017 16:43:56: Fri Nov 03, 2017 16:43:56: Exception occured at: 0x20000280 Fri Nov 03, 2017 16:43:56: Fri Nov 03, 2017 16:43:56: See the call stack for more information. Fri Nov 03, 2017 16:43:56: Unloaded macro file: C:\Program Files (x86)\IAR Systems\EWARM8\arm\config\flashloader\ST\FlashSTM32H7xxx.mac Fri Nov 03, 2017 16:43:58: IAR Embedded Workbench 8.20.1 (C:\Program Files (x86)\IAR Systems\EWARM8\arm\bin\armproc.dll) =============================================================================So, I was checking this file.
Line 203 : if ((dbgmcu_cr &((0x3<<7) | (0x7<<0)) != ((0x3<<7) | (0x7<<0))) {
I think that need modify this sentence.
such as : if ((dbgmcu_cr &((0x3<<7) | (0x7<<0))) != ((0x3<<7) | (0x7<<0))) {
Please confirm me!
#dmac #iar #stm32h72018-08-09 9:53 PM
Sorry, bumping old zombie unanswered questions off my feed
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.