2016-10-20 2:13 AM
Hi,
I have the following routine for writing to EEPROM which checks whether the data to be written matches the current EEPROM contents. If there is no match, the EEPROM contents are erased and the new data is written.// Enable writing to EEPROM
DATA_EEPROM_Unlock();// Iterate through data to be written, find where it differs from EEPROM
// contentsand only re-program where needed for ( Index = 0u ; Index < LengthRAM ; ++Index ) { // Check whether contents of EEPROM already match the data to write if ( pEEPROM[Index] != pRAM[Index] ) { // Get the address to write to in EEPROM uint32_t WordAddress = (uint32_t)&pEEPROM[Index]; TryCount = 0u ; status = FLASH_ERROR_WRP ; while ( status != FLASH_COMPLETE ) { // Clear flash flags FLASH_ClearFlag(FLASH_FLAG_EOP|FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLAG_SIZERR | FLASH_FLAG_OPTVERR); // Erase word in EEPROM status = DATA_EEPROM_EraseWord( WordAddress ) ; ++TryCount ; // Check that EEPROM has been erased in a reasonable time BSP_ASSERT( 10u > TryCount ) ; } // Write new data to EEPROM status = DATA_EEPROM_ProgramWord( WordAddress, pRAM[Index] ) ; BSP_ASSERT( FLASH_COMPLETE == status ) ; } }Recently the functionDATA_EEPROM_EraseWord()
has been returningFLASH_ERROR_PROGRAM
on every attempted erase, causing the program to assert a few lines later.There haven't been any updates to the code responsible for managing the EEPROM, this code was working before, but I have now seen the issue on multiple devices. Is it possible that the EEPROM has been worn out by too may writes? What does the value FLASH_ERROR_PROGRAM signify? Any help would be greatly appreciated. #eeprom #stm32l1522016-10-21 6:38 AM
Hello,
Could you please provide details about your environment ? What compiler and debugger are you using? RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.