2025-12-30 2:57 AM - last edited on 2025-12-30 3:04 AM by Andrew Neil
Suppose I have a project where I have to continuously read and display values from the adc called AD9215BRUZ, I have NUCLEO-H753ZI board , is it possible? Can the STM Hseries read and sample parellel data , if yes then how should I proceed , if no then what are the limitations.
Thank you
Solved! Go to Solution.
2025-12-30 3:13 AM
yes, it’s possible, but not via the STM32’s internal ADC.
The AD9215 outputs parallel LVTTL data. The STM32H753 can read this using GPIOs with a timer/DMA or the FMC (FSMC) interface, depending on your sampling rate.
How to proceed:
Limitations:
If you need very high sustained rates, an FPGA is usually the better choice.
2025-12-30 3:05 AM - edited 2025-12-30 3:22 AM
Hello @-__- and welcome to the ST community,
The only parallel interface available on STM32H753 is the FMC interface. but you need to read AD9215 datasheet and study the signals to confirm if this is doable.
With other H7 series (Ex: STM32H72x/H73x), PSSI interface is available for parallel communication you need also to confirm by reading AD9215 datasheet.
Otherwise, you can handle that with GPIOs (+ eventually DMA transfers from to GPIOs + a timer triggering DMA transfers for a synchronous communication)
2025-12-30 3:13 AM
yes, it’s possible, but not via the STM32’s internal ADC.
The AD9215 outputs parallel LVTTL data. The STM32H753 can read this using GPIOs with a timer/DMA or the FMC (FSMC) interface, depending on your sampling rate.
How to proceed:
Limitations:
If you need very high sustained rates, an FPGA is usually the better choice.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.