2026-01-30 5:07 AM
Would writing to the crossbar registers (SETx1R, RSTx1R, SETx2R, RSTx2R of all 6 timers) on every PWM cycle (max 200kHz) affect long term reliability? I'm running this in an interrupt routine for a power converter and I'm wondering if doing this would make sense to have a more consistent processor delay. Preload is enabled on all 6 timers and master timer. Register updates on timers 1-6 occur on master timer register update.
Solved! Go to Solution.
2026-01-30 8:05 AM
Writing to register won’t affect reliability. You’re not going to wear things out, if that is the concern. The registers are not like flash where there is a limited number of read/write cycles.
2026-01-30 5:20 AM
Hello,
I'm wondering why writing to registers in the MCU would affect the reliability? reliability implies to the Flash not to the registers.
2026-01-30 8:05 AM
Writing to register won’t affect reliability. You’re not going to wear things out, if that is the concern. The registers are not like flash where there is a limited number of read/write cycles.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.