2020-11-19 1:03 AM
Hi everyone,
I am trying to read a laser sensor through UART of STM32F4 inside Simulink. The laser sensor's refresh rate is 10 Hz approximately but it does not give the data periodically. I am using UART Interrupt for reading action. There are two cases:
->If I read it byte per byte, then I can not receive the laser data in necessary order. It is received randomly.
->If I read it by defining a buffer inside UART, depending on the size of the buffer, it is filled correctly but this time because of randomness in byte per byte case, the refresh of the data is not at the desired level.
Probably either because of Simulink's built in code for UART or because of something that I don't understand, the reception is not at the desired level. I am open to any suggestions and help.
2022-08-13 6:56 AM
Hi CSutu,
I am new also trying to read data with Simulink - Did you figured out the solution ? if yes could please share how to do it ?
many thanks,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.