2016-02-26 4:57 AM
Dear Madams and Sirs,
im trying to programming / and reading an 1Mbit EEprom with STM32F030x. There are some issues i am working on and make me some headache. Im using the STM32f0xx_i2c files for working and a Keil Compiler (V5.17). My first problem is: Im using one of our internal libarys to write and read to the eeprom. It is programmed as discriebed in the the STM Reference Manual and worked fine with EEprom values lower 1Mbit. I added a second adress byte to the adressing and put the value of sending bits in the I2C_TransferHandling to 2. But when im looking to the data with a Osciloscop I see only one adress byte. In case of writing it seems that the 2nd one is puting to data (because i have to rise the data by one to the former version). In case of reading the start byte / device select byte for reading will be send after the 1st Adressbyte. The 2nd adress byte is missing. The other issue is: When im putting the 2nd Adress byte to the code the routine will not more handle the waiting for the TXIS flag after setting I2C_TransferHandling at the start. It looks like hanging up there. This work also fine, when i'm only using one byte of adressing. I try to programm the routine new, in a different way - by using I2C_SlaveAddressConfig(); I2C_NumberOfBytesConfig(); I2C_SendData() and try it a the write routine. This didn't work either with the same result. the starting routing stopps after the first adress byte. Does somebody has an example for this task or an idea what is going wrong? Kind regards Jens #i2c #eeprom #1mbitWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.