2025-04-08 8:45 PM - last edited on 2025-04-09 2:19 AM by Andrew Neil
I using STM32duino to program the STM32F103C8T6. When I use the Seiral1 to communicate with a 4G, the data reveived exceeds 64 characters, data will lost. By using modify the following #defines, it does not working. I am appreciated if somebody could help. The folowing test prgram file is as following:
2025-04-08 11:04 PM
Here you can find help and advice on your project.
2025-04-09 2:23 AM
Please see How to insert source code.
@caixf wrote:I using STM32duino
Then this is the place to post: https://www.stm32duino.com/
Maybe also in the Arduino forums: https://forum.arduino.cc/
Note that these forums will also have requirements for posting source code to keep it legible.
2025-04-09 7:06 AM
Thank you for your information.
2025-08-29 1:35 AM - edited 2025-08-29 1:36 AM
When you define in the sketch file (.ino) it is not defined globally as it is converted as a .cpp file.
To properly redefine the
SERIAL_RX_BUFFER_SIZEyou have to create a file named build_opt.h and add:
-DSERIAL_RX_BUFFER_SIZE=1024Like this is properly redefined globally.
See the wiki for more information.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.