2025-04-16 2:48 AM - edited 2025-04-16 11:27 AM
Hello,
I'm learning embedded development (junior level) and picked up a free STM32u575zit6q Nucleo Dev Board.
My goal is to build an embedded system that captures a VIN string and saves it to a .csv file. Ideally done through embedded and low level. Later I'd like to incorporate cloud systems to easily see the csv as a spreadsheet on an app or webpage and phase out the LCD/IPS display.
My main question is, how important is an FIFO for this board and would it hurt if I don't buy a camera that has one installed? What cams would be ideal for this project?
Is there a system for scanning VINs and converting them to strings easily? I was thinking of incorporating Yolo/OpenCV but not sure if this microprocessor would be powerful enough.
Any advice on my design choices?
Display:
2.4 inch SPI onilne shop factory ESP32 LCD TFT Electronic Module colorful RGB 65k ILI9341 Display 320*240
Camera Module:
b_u585i_iot02_: when looking through the projects, I noticed the STMU5 already had some camera driver support
B-CAMS-OMV Camera Module STMicroelectronics camera module (MB1379)
– Based on the OV5640 image sensor offering a 5-Mpixel resolution with 8-bit color
This however was my first choice until I noticed the importance of an FIFO for an STM32
OV7670 300KP camera module module Supports VGA CIF auto exposure control display active size 640X480 For Arduino
or the Rasp Pi/Adrucam 12 MP IMX477*
When choosing a camera module, what am I looking for? If it's DCIM or STM32 compatible or just forums and documentation?
If you could explain why both the ST cameras are HQ 5 MP but look extremely different that'd be helpful.
Thank you,
Dan (blurry)
Solved! Go to Solution.
2025-04-22 5:41 AM
Hello @blurry and welcome to the community;
To know if a CMOS sensor (a camera module) is compatible with the DCMI or not, the user must check the following points in the CMOS sensor specifications:
• Parallel interface (8-, 10-, 12-, or 14-bit)
• Control signals (VSYNC, HSYNC, and PIXCLK)
• Supported pixel clock frequency output
• Supported data output
The AN5020 mentioned some examples of supported camera by STM32 DCMI.
There is a wide range of camera modules and CMOS sensors that are compatible with the STM32 DCMI.
The table below lists some of them.
I recommend you to look at AN5020 "Introduction to digital camera interface (DCMI) for STM32 MCUs". This application note gives to the STM32 users some basic concepts, with easy-to-understand explanations of the features, architecture, and configuration of the DCMI. It is supported by an extensive set of detailed examples.
I hope this help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-22 5:41 AM
Hello @blurry and welcome to the community;
To know if a CMOS sensor (a camera module) is compatible with the DCMI or not, the user must check the following points in the CMOS sensor specifications:
• Parallel interface (8-, 10-, 12-, or 14-bit)
• Control signals (VSYNC, HSYNC, and PIXCLK)
• Supported pixel clock frequency output
• Supported data output
The AN5020 mentioned some examples of supported camera by STM32 DCMI.
There is a wide range of camera modules and CMOS sensors that are compatible with the STM32 DCMI.
The table below lists some of them.
I recommend you to look at AN5020 "Introduction to digital camera interface (DCMI) for STM32 MCUs". This application note gives to the STM32 users some basic concepts, with easy-to-understand explanations of the features, architecture, and configuration of the DCMI. It is supported by an extensive set of detailed examples.
I hope this help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.